news 1 week ago

Prosecutor: Weinstein saw victims as 'complete disposables'

The Associated Press — By MICHAEL R. SISAK and TOM HAYS - Associated Press

NEW YORK (AP) — Harvey Weinstein considered himself such a big shot in Hollywood that he thought he could get away with treating aspiring actresses like "complete disposables," a prosecutor told a jury in closing arguments Friday at his New York City rape trial.

“The universe is run by me, and therefore, they don't get to complain when they are stepped on, spit on, demoralized and, yes, raped and abused by me — the king," Assistant District Attorney Joan Illuzzi-Orbon said, mimicking Weinstein.

Using a TV monitor next to the jury box, the prosecutors displayed photos of “Sopranos” actress Annabella Sciorra and five other accusers who also testified. Illuzzi told jurors that, putting aside the more successful Sciorra, who dined with Uma Thurman and dated Gary Oldman, the women were viewed by Weinstein as “complete disposables.”

“These other women, they were never in his world,” Illuzzi said. “They are never going to be in his world. They are never going to be strong enough, bold enough or brave enough to tell. But Annabella — someone might believe her.”

Illuzzi also showed a side-by-side comparison of Sciorra's testimony about confronting Weinstein in the mid-1990s — after she accuses him of raping her — and similar testimony by the woman he's charged with raping in 2013 about how the mogul reacted when she told him she had a boyfriend.

“His eyes went black and I thought he was going to hit me right there,” Sciorra testified. With the click of a button, the rape accuser’s testimony popped up: “His eyes changed and he was not there. They were very black and he ripped me up.”

At times, Weinstein sat back in his chair staring ahead at a screen in front of the defense table that mirrored what was being shown to the seven men and five women on the jury.

After sitting through the three-hour summation, Manhattan District Attorney Cyrus Vance Jr. shot reporters a thumbs up. Meanwhile, Weinstein's lawyers said the film producer was confident, heading into the long weekend before the start of deliberations Tuesday.

“The evidence is all on our side,” Weinstein's lawyer Donna Rotunno said.

Illuzzi's closing comes a day after Rotunno offered an epic, hourslong defense closing argument, painting the prosecution's case as a “sinister tale” absent proof needed to convict Weinstein.

Prosecutors created an “alternate universe” that “strips adult women of common sense, autonomy and responsibility," Rotunno argued.

“Regret does not exist in this world, only regret renamed as rape," she said.

Illuzzi pushed back Friday as she described Mimi Haleyi’s allegations that Weinstein held her down on the bed and forcibly performed oral sex on her in his SoHo apartment in 2006.

“When an adult goes to another adult’s home, should they expect that they are going to have to engage in sex?" the prosecutor asked.

"By going to Harvey Weinstein's home, did she deserve what she got?”

“There are no blurred lines here,” she added. “This is a crime.”

Weinstein, 67, is charged with raping a woman in a Manhattan hotel room in 2013 and forcibly performing oral sex on Haleyi in 2006. Jurors can consider Sciorra's allegation in weighing charges alleging that Weinstein is a sexual predator, even though it is too old to be charged on its own.

The Associated Press has a policy of not publishing the names of people who allege sexual assault without their consent; it is withholding the name of the rape accuser because it isn’t clear if she wishes to be identified publicly.

Other accusers testified as part of a prosecution effort to show he used the same tactics to victimize many women over the years.

In response to defense claims that Haleyi and the woman he's charged with raping were opportunists who had consensual sex with Weinstein because they thought it would help their careers, prosecutors are seeking to focus the jury's attention on harrowing accounts alleging rapes, forced oral sex, groping, masturbation, lewd propositions and casting-couch experiences.

Some women testified that Weinstein ignored pleas of “no, no, no” as he assaulted them. The woman Weinstein is charged with raping said he would turn violent when he couldn't get his way and that “if he heard the word no, it was like a trigger for him."

Another woman recalled Weinstein sneering, "You’ll never make it in this business; this is how this industry works,” when she laughed off his advances.

The prosecution’s task has been complicated because the women he is charged with raping kept in contact with Weinstein after the alleged encounters. But Illuzzi said part of his scheme was to keep in contact with them so he could point to those encounters as evidence nothing happened, essentially “preparing for a moment just like this.”

Case in point, she said: In October 2017, Weinstein replied to an email from a publicist giving him a heads up that Sciorra was about to go public by writing: “Annabella did cop land.”

That was a reference to a 1997 Weinstein-produced movie that Sciorra acted in. She said she didn’t realize when auditioning that his studio was involved.

Instructing his publicist on how to respond to the article, Weinstein wrote: “this was consensual or deny it.”

“I submit to you that was a confession,” Illuzzi told jurors over the defense’s denied objection.

___

On Twitter, follow Michael Sisak at twitter.com/mikesisak and Tom Hays at twitter.com/aptomhays

___

For more coverage visit apnews.com/HarveyWeinstein