Pablo Larrazábal keeps top spot at Leopard Creek
The Associated PressMALELANE, South Africa (AP) — Pablo Larrazábal kept his three-shot lead at the Alfred Dunhill Championship on Saturday ahead of the final round of the European Tour’s 2020 season-opener.
Larrazábal’s 2-under 70 in the third round put him 11 under par and kept him ahead of Wil Besseling (70). South African home favorite Branden Grace (71), the 2014 champion, slipped a shot further back to third on 7 under.
Larrazábal made five birdies but also three bogeys on another tough day at Leopard Creek Country Club, where players have faced scorching temperatures pushing 40 degrees Celsius (104 Fahrenheit) and gusting winds.
Those high temperatures convinced the tour to allow players to wear shorts in tournament play for the first time.
“I hung in there and we will see, it will be a fun Sunday afternoon,” said Larrazábal, who won the last of his four European Tour titles four years ago. “If I shoot in the 60s these guys are going to have to put some run on me tomorrow.”
Former Masters champion Charl Schwartzel is making a solid return after an eight-month injury layoff because of a wrist problem. A 70 put him 4 under and in a tie for sixth at the tournament he’s won a record four times.
Zander Lombard (69) and Marcus Armitage (71) are a shot ahead of Schwartzel’s group in fourth.
___
More AP golf: https://apnews.com/apf-Golf and https://twitter.com/AP_Sports