news 1 week ago

Freshen Up Your Pearly Whites With One of These Top-Notch Electric Toothbrushes

StackCommerce — shannon

Whether you’re meeting someone for the first time, heading to a job interview, or simply hanging out with friends, donning a yellow smile can really be a turn-off. Sure, you could cut back on the red wine and coffee, but perhaps the problem lies in your toothbrush. Regular, disposable toothbrushes aren’t always able to remove the plaque and stains from your teeth the way electric ones can. 

But with high-quality electric toothbrushes often costing upwards of $100 bucks, it’s hard to give in and take the plunge. Well, until now, that is. We’ve found three incredible electric toothbrushes that will give you that just-went-to-the-dentist feeling after every single brush at a deeply discounted rate. Seriously. 

1. The Aquasonic PRO Toothbrush

If electric toothbrushes could be superheroes, this Aquasonic PRO Toothbrush would be the star in every Marvel movie ever made. That’s because this toothbrush literally zaps plaque from your teeth in practically a blink of an eye. Boasting an incredible 40,000 vibrations per minute, the Aquasonic PRO Toothbrush completely eliminates plaque from your teeth and gums. When using the tool, you’ll have four different brushing modes to choose from (clean, soft, whiten, or massage ) depending on your comfort level. 

And that’s all just the tip of the iceberg. This innovative toothbrush also features a smart vibration timer that alerts you when you’re done brushing, ensuring you get the absolute most from your cleaning sessions. Additionally, the tool’s adaptive brush head can switch back and forth from polishing tooth enamel to gently massaging the gums without you even noticing.

This larger-than-life electric toothbrush also comes with a wireless charging glass that effortlessly juices up the device in between uses. You can even use the glass to rinse your mouth out with. And its included carrying case ensures you never have to go a day without an incredible brush, no matter where you are.

The deal: The Aquasonic PRO Toothbrush with 6 ProFlex Brush Heads, Wireless Charging Glass & Case is now 45% off at just $54.99.

2. The Platinum Sonic Toothbrush & UV Sanitizing Charging Base

If you knew the kind of bacteria that grows on toothbrushes in between uses, you’d likely never touch one again. That’s why germaphobes and health-enthusiasts everywhere are buzzing about this Platinum Sonic Toothbrush and its UV sanitizing charging base. But aside from its germ-killing capabilities, this electric toothbrush leaves your mouth feeling incredibly clean every time you use it. 

First off, the brush features incredible polishing power, complete with bristles that buzz at a whopping 40,000 vibrations a minute. You’ll also get to choose from four brushing modes: clean, dazzle, and pulse.  This electric toothbrush gets rid of stubborn plaque with gentle yet great force, leaving you with polished, pearly whites. And with the brush’s programmed 30-second area-change alerts, you’ll never cheat your teeth of a proper clean.

What truly sets this brush apart from others like it on the market is its UV sanitizing charging base. Not only does this base juice up your brush so it’s always raring to go, it actually kills germs and bacteria festering on the brush. Now that’s clean! 

The deal: Get the Platinum Sonic Toothbrush & UV Sanitizing Charging Base With 2 Bonus Brush Heads in rose gold for just $49.99 — that’s 80% off!

3. The TAO Clean Sonic Toothbrush & Cleaning Station 

If you love good, clean, sanitizing fun, this TAO Clean Sonic Toothbrush & Cleaning Station is right up your alley! Not only does this thing give your mouth a level of clean you only ever feel after visiting the dentist, it also cleans itself in between uses thanks to its powerful UV-C rays.

When using this electric toothbrush, you’ll have the option of using two different easy-to-control modes, professional and sensitive, along with zone-changing alerts that ensure you get enough brushing. The brush also vibrates at 40,000 strokes per minute and uses state-of-the-art sonic technology, giving you a thorough clean you just can’t get with a regular toothbrush. 

Sure, that’s all impressive and all, but what really makes this toothbrush one-of-a-kind is its self-cleaning capabilities. When you’re done brushing, simply stick the brush — bristle end down — into its accompanying base. Once it’s in there, ultra-violet rays hit the brush at every angle, killing 99% of germs and drying the brush. If that doesn’t make you smile, what will?

The deal: Get the TAO Clean Sonic Toothbrush & Cleaning Station in rose gold for the discounted price of just $69.99!

Like this deal? Check out Vault — you’ll get four premium tools, including NordVPN and Dashlane, to supercharge your online security. Try it free for 14 days now!

All prices subject to change.