news 1 month ago

With Car Gadgets Like These, You’ll Start Looking Forward to Sitting in Rush Hour

StackCommerce — shannon

On a daily basis, you spend a lot of time in the car. Whether it’s commuting to work, dropping off your kiddos’ carpool, or running errands, your car can sometimes feel like a second home. So why not spruce things up a bit? There are all kinds of great gizmos and gadgets out there that can turn a boring drive into an exciting one, like cup-holder humidifiers, wireless chargers that work at lightning speeds, and top-notch on-the-go emergency kits. Who knows, your dreaded rush-hour may turn into your favorite time of the day. 

Take a look at these freshly discounted car accessories and gadgets ideal for long and short drives alike.

1. The Car Cup Humidifier

Smell that? It’s the stale aroma from last night’s Chinese take-out you picked up after work. Lingering car odors are never pleasant and for some reason, they’re extremely hard to get rid of — until now, that is. Say hello to the Car Cup Humidifier, an ingenious gadget that humidifies the air in your car, diffuses odors, and even serves as a handy LED light, ideal for nighttime cruising.

While this humidifier is small enough to fit in your car’s cupholder, its power can’t be matched. The little gadget effortlessly humidifies the air with a 230ml water capacity and a 35ml per hour mist output. That’s why it can also work great in your office, bedroom, hotel room and wherever else you decide to take it. And thanks to its attached LED light, you can make sure it matches your surroundings perfectly. 

At 52% off, this Car Cup Humidifier is an absolute must-have! Snag one for yourself for just $19 bucks.

2. The Hudly 10 W Fast Wireless Car Charger & Mount

These days, navigating around town hands-free is the law, which is why a great car phone mount is ideal. But why not step things up a notch with a mount that charges your phone at record fast speeds? The Hudly 10 W Fast Wireless Car Charger can do just that. Holding your phone safely and securely with its non-scratch silicon arms, this mount can simultaneously charge your phone without requiring you to touch a single wire. 

Simply stick the mount into your car vent, dashboard or windshield and enjoy fantastic viewing angles with 360º rotation abilities. The mount even boasts an additional USB port so you can charge two devices at a time. While all its features are impressive, its fast-charging capabilities are what really set it apart from other mounts like it. No matter how long or short your ride is, you can ensure your Qi-compatible devices are always juiced up to the max without worrying about overheating or short-circuiting. And when you’re done using the mount, press its handy quick-release button to retrieve your device.

For a limited time, the Hudly 10 W Fast Wireless Car Charger & Mount is on sale for just $30 bucks!

3. The Ztylus Stinger Car Charger Emergency Tool

Just as Clark Kent turns into Superman when disaster strikes, this phone charger effortlessly transforms into a life-saving car emergency tool in the direst situations. While you can use the Ztylus Stinger Car Charger Emergency Tool as an everyday charger, it also provides you with everything you’d need if you were stuck in your car and needed to get out, fast. 

Unlike other emergency car tools, this is one you can use every single day as a charger so it’s always within reach when you really need it. This smart gadget boasts two USB ports so you can charge multiple devices at a time. Simply pop it into your car’s cigarette lighter and it’s ready to get to work. And if disaster strikes, the little charger features a razor-sharp cutter capable of slicing through a 5000-lb tow strap! Needless to say, it’ll cut your seatbelt in a jiffy. It also boasts a highly effective spring-loaded glass breaker so you can shatter your car’s window in mere seconds if necessary. 

Be prepared for whatever comes your way on the road with the Ztylus Stinger Car Charger Emergency Tool now just $19.95.

Like these deals? Check out Vault — you’ll get four premium tools, including NordVPN and Dashlane, to supercharge your online security. Try it free for 14 days now!

Prices subject to change.