Advertisement

Now Playing

Bryan Cranston On Wearing Hazmat Suits at Comic-Con and Emmy Morning

Bryan Cranston On Wearing Hazmat Suits at Comic-Con...

Breaking Bad is back tonight! The show kicked off season five at Comic-Con last night with a special screening of the season opener, and we were on the red carpet to chat with Walter...

Most Popular PopSugarRush Videos

Previous Next
Back to All Channels

Browse PopSugarRush Videos

Andrew Supports Emma at Cancer...

May 22 - Andrew Garfield and Emma Stone are continuing their...

runtime: 02:24

We Had the Cast of Fast &...

May 22 - We were at the red carpet premiere of Fast & Furious 6...

runtime: 03:46

Wiz Khalifa on the Fast &...

May 22 - Wiz Khalifa teamed up with 2 Chainz for a track on the...

runtime: 01:42

Watch, Pass, or Rent Video...

May 22 - Paul Walker, Vin Diesel, and Dwayne Johnson return to...

runtime: 03:00


Luke Evans on Joining the Fast...

May 22 - Luke Evans plays the villain in Fast & Furious 6, but...

runtime: 01:20

Michelle Rodriguez on Coming...

May 22 - Michelle Rodriguez's character may have gotten killed...

runtime: 02:16

Jennifer Aniston Tries Talk...

May 22 - Jennifer Aniston plays cohost on today's episode of The...

runtime: 02:47

Fast and Furious 6 Star Elsa...

May 22 - Last night Fast and Furious 6 premiered in LA last night...

runtime: 01:57


Up-and-Coming Actress Julia...

May 22 - Actress Julia Garner is at the Cannes Film Festival for...

runtime: 04:37

Jaden Smith on the Perks of...

May 22 - At 14, Jaden Smith has already made two feature films...

runtime: 02:04

Watch, Pass, or Rent Video...

May 22 - The Wolfpack returns for one last crazy adventure in The...

runtime: 03:26

Matt Damon Talks "Jarring"...

May 21 - The beaches in the South of France are known for their...

runtime: 03:35