Advertisement

Now Playing

Colin Farrell on "So Tough" Jessica Biel - "I'm Glad I Don't Fight Her!"

Colin Farrell on "So Tough" Jessica Biel - "I'm...

It sounds like Kate Beckinsale and Jessica Biel struck the fear in Colin Farrell on the Total Recall set. Colin spoke to us at Comic-Con today about both of his tough leading ladies and...

Most Popular PopSugarRush Videos

Previous Next
Back to All Channels

Browse PopSugarRush Videos

Andrew Supports Emma at Cancer...

May 22 - Andrew Garfield and Emma Stone are continuing their...

runtime: 02:24

We Had the Cast of Fast &...

May 22 - We were at the red carpet premiere of Fast & Furious 6...

runtime: 03:46

Wiz Khalifa on the Fast &...

May 22 - Wiz Khalifa teamed up with 2 Chainz for a track on the...

runtime: 01:42

Watch, Pass, or Rent Video...

May 22 - Paul Walker, Vin Diesel, and Dwayne Johnson return to...

runtime: 03:00


Luke Evans on Joining the Fast...

May 22 - Luke Evans plays the villain in Fast & Furious 6, but...

runtime: 01:20

Michelle Rodriguez on Coming...

May 22 - Michelle Rodriguez's character may have gotten killed...

runtime: 02:16

Jennifer Aniston Tries Talk...

May 22 - Jennifer Aniston plays cohost on today's episode of The...

runtime: 02:47

Fast and Furious 6 Star Elsa...

May 22 - Last night Fast and Furious 6 premiered in LA last night...

runtime: 01:57


Up-and-Coming Actress Julia...

May 22 - Actress Julia Garner is at the Cannes Film Festival for...

runtime: 04:37

Jaden Smith on the Perks of...

May 22 - At 14, Jaden Smith has already made two feature films...

runtime: 02:04

Watch, Pass, or Rent Video...

May 22 - The Wolfpack returns for one last crazy adventure in The...

runtime: 03:26

Matt Damon Talks "Jarring"...

May 21 - The beaches in the South of France are known for their...

runtime: 03:35