news 1 week ago

Simpson ties course record, takes 5-shot lead at Players

The Associated Press — By DOUG FERGUSON - AP Golf Writer

PONTE VEDRA BEACH, Fla. (AP) — No one ever played a better round at the TPC Sawgrass than Webb Simpson.

For 16 holes, anyway.

With his sixth straight birdie on the back nine, Simpson became the first player to reach 11-under par for a single round at The Players Championship. The course record? Simpson couldn't resist thinking about a 59. All he had to do was navigate the shortest and scariest hole Friday afternoon on the Stadium Course.

He hardly missed anything all day except the island green on No. 17.

Splash!

"Just the wrong club," he said.

The consolation was enormous. Even with that double bogey, Simpson tied the Stadium Course record with a 9-under 63 and had a five-shot lead after 36 holes, the largest in the 45 years of this tournament.

"Everything is going in," he said. "You feel like no matter what, you're going to make it, and I grew up on an easy golf course so it reminded me of being back home, shooting low numbers. But at the same time, you're at the TPC Sawgrass, so you know that trouble is everywhere, as you guys saw with me on 17."

The sand wedge in the water on the 17th ruined his round, but not his day. Simpson couldn't miss putts he wasn't even trying to make, whether it was a 35-foot eagle putt on his second hole or a 30-foot birdie putt up the slope and into the cup on the 15th .

At that point, all he could was laugh.

And then he reached the 17th, playing 147 yards to a back pin, the light wind playing tricks with him. He kept backing off, consulting with his caddie as he tried to decide between sand wedge and pitching wedge.

"The wind seemed to be changing," he said, "and people were yelling at me to hit it."

The ball hit the wooden frame on the front of the green, caromed high in the air and landed on the back of the green with so much momentum that it rolled through the light collar of rough and disappeared into the water.

Simpson was the seventh player to shoot 63 on the Stadium Course — five since 2013 — and his 15-under 129 tied the 36-hole record set two years ago by Jason Day.

Charl Schwartzel (66), Patrick Cantlay (68) and Danny Lee (66) were five shots behind.

Tiger Woods at least gets to return on the weekend. He made the cut on the number (1-under 143) after a 71 in the easier morning conditions. Woods was outside the cut line until Jordan Spieth and Justin Thomas each made bogey on the 18th. Spieth three-putted from 35 feet, though he shot 68 and ended three straight years missing the cut. Rory McIlroy wasn't so fortunate. He was inside the cut line until hitting into the water on the 17th and making double bogey.

Conditions were ideal for scoring for the second straight day. Simpson took that to another level.

He ended the front nine with a 15-foot birdie putt on the par-5 ninth for a one-shot lead, and then he took off. Starting with an up-and-down at the par-5 11th, Simpson ran off six straight birdies — three straight from the 20-foot range, the most unlikely birdie with the one from behind the 15th green, and another up-and-down from left the of the green on the par-5 16th.

Spieth was 5 under on his round through 11 holes and wondered if he had the low round of the day. And then he saw a leaderboard.

"It was just amazing," said Spieth, who played with McIlroy and Thomas. "We were talking about it throughout the round, all three of us. We were like, 'Man, I hope he shoots 59.' And at the same time, we're saying if he shoots 59, can you imagine how hard the setup is going to be tomorrow?"

The real challenge will be catching Simpson.

Only three other players have led by as many as three shots through 36 holes at The Players — Lanny Wadkins (3) in 1979, Greg Norman (3) in 1994 and Day (4) in 2016. All of them went on to win.

"If you're off a little bit, you make bogeys or double bogeys as easy as you can make birdies," Simpson said. "I don't think any lead is safe."

Schwartzel never came close to a bogey, only missing two greens, and just barely. Cantlay only had one bad swing and one bad break, both on the par-5 ninth, that led to bogey. Lee shot a 31 on the back nine with a double bogey on the 11th hole.

Simpson left them all in his wake.

"The most entertaining golf in our group was watching Webb's score," said Justin Rose, who played behind Simpson and shot 72. "It's a miracle round. To be 11-under par, it's a shame he doesn't finish it off. But 17 is a hard hole to get through. I'm sure he was nervous playing that hole. We're all nervous playing that hole, but an 11-under par round, that green I'm sure looks even smaller."

Woods had wedges in his hand on his opening three holes and never got it close for birdie, and it was like that all day. He was in the feature pairing with Phil Mickelson and Rickie Fowler, and Woods was the only one to make the cut.

Mickelson went 79-73 and missed the cut for the fifth time in the last six years. Fowler was in good shape until losing a ball in a tree on the sixth hole for the first of consecutive double bogeys. He shot 71 and missed by two shots.

AdChoices