Free Online Games: Dibbles 4: A Christmas Crisis

Close

The Dibbles return once again, but this time our King is on a new Christmas themed mission. Command the Dibbles and help their king safely cross 33 Xmas themed levels. What's so important to him that he needs hundreds of his loyal subjects to lay down their lives this time? You'll just have to complete the game and find out! New features include: - Slippy, slidey ice - New Xmas pressies that get in the way and can be moved around to form part of the solution - New "Swan Dive" command - New "Ramp" command - Multiple start and finish locations on some levels Merry Christmas!

Close Use the mouse to select from the available commands and place command stones on the level. The first Dibble to encounter the command will pick it up and when the opportunity arises, he'll carry it out - even if it means sacrificing his life (which is almost certainly the case).
Close Controls not available.
Average Rating: