SWTOR Subscriber Base Shrinks

Also available for : PC

Electronic Arts reported a drop in Star Wars: The Old Republic's subscriber base, down to 1.3 million from the <b><a target="_blank" href="http://pc.ign.com/articles/121/1217723p1.html" target="_new">1.7 million figure given in February 2012</b></a>.<br/><br/>This news comes after the release of Star Wars: The Old Republic's 1.2 Legacy update, which added a large amount of new content to the game including dungeons, a PvP arena, and incentives to start new characters and replay content as different classes.<br/><br/><iframe width="467" height="267" src="http://www.youtube.com/embed/1Tm552u-OaU" frameborder="0" ></iframe><br/><br/>Star Wars: The Old Republic is a subscription-based MMO and requires active players to pay 15 USD per month after purchasing the base game, which starts at 60 USD. As of the end of April 2012, 2.4 million units of Star Wars: The Old Republic have sold through.<br/><br/>Despite the lower subscriber numbers, EA considers Star Wars: The Old Republic to be the number two MMO in the West, and says it's stable and profitable. Most of the subscriber number drop was attributed to the loss of more casual players. Expect more of an emphasis on elder game PvP and guild features moving forward in 2012.<br/><br/>BioWare also hinted at what's in store for the upcoming <b><a target="_blank" href="http://pc.ign.com/articles/122/1222459p1.html" target="_new">1.3 update</b></a>. <br><br/><br/>&#169;2012-05-07, IGN Entertainment, Inc. All Rights Reserved