The Elder Scrolls V: Skyrim (Collector's Edition)

Also available for: PS3

The Empire of Tamriel is on the edge. The High King of Skyrim has been murdered. Alliances form as claims to the throne are made. In the midst of this conflict, a far more dangerous, ancient evil is awakened. Dragons, long lost to the passages of the Elder Scrolls, have returned to Tamriel. The future of Skyrim, even the Empire itself, hangs in the balance as they wait for the prophesized Dragonborn to come; a hero born with the power of The Voice, and the only one who can stand amongst the dragons.<P>The Collector's Edition of Skyrim includes an Alduin statue, an official art book, and a Making of The Elder Scrolls V: Skyrim DVD.

Release Date: 11/11/2011

Genre: RPG

ESRB Rating: M

Screenshots

Games Ratings

No Data Available